(0)| 6/18/2010 5:09 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello S.S.D.D.; Have a look at the answers provided elsewhere in the forum: From the S5 to S7 conversion manual: Which parts of your program should be reprogrammed in S7? … Absolute addresses cannot be addressed in S7. The corresponding instructions (such as LIR, TIR, etc.) are not converted. If a program frequently works with absolute addresses, it is a good idea to rewrite these parts of the program or, if necessary, the entire program .… Have a look at this thread: /tf/WW/en/Posts/33637 Look at Phantom’s and simaticus’ replies in this thread: /tf/WW/en/Posts/12597 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/18/2010 5:09 PM |
|
Follow us on