(0)| 6/22/2010 4:22 PM | |||
|
Joined: 9/27/2006 Last visit: 12/31/2025 Posts: 12479 Rating:
|
Hello giang; The best source of information on the USS protocol for the S7-200 CPUs is the S7-200 Programmable Controller System Manual, that you can download here: http://support.automation.siemens.com/WW/view/en/1109582 Chapter 11 is dedicated to the USS protocol with MM4 drives.It contains explanations of the protocol, programming instructions and drive parameters for configuring USS. You will also find there the part number for the Modbus/USS add-onprotocol libraries, that you must purchase for integration to MicroWin:
Daniel Chartier |
||
| 6/23/2010 8:23 AM | |
|
Posts: 2930 Rating:
|
Hi, in addition to the information in the S7-200 system manual there are also examples available for download free of chanrge. All examples use a SI`NMAIC G110 but shouls also work with MM420. Here you can find the examples: http://support.automation.siemens.com/WW/view/en/35125712 I hope this helsp |
| 6/23/2010 3:12 PM | |
|
Joined: 1/17/2006 Last visit: 12/28/2025 Posts: 555 Rating:
|
Hello Giang, In the following links you can find informations about the comm of S7-200 and MM4 using USS protocol with example. S7200_MM4_USS_Connection MicroSet Tip 28 MicroSet Tip 65 And following a link with S7-200 and SINAMICS G110, very good doc. Micro Automation: Simple networking and cascading of drives (MAS 26) I hope this helps you ! |
| 12/2/2014 10:02 AM | |
|
Joined: 9/1/2005 Last visit: 10/31/2025 Posts: 4114 Rating:
|
follow up question published by silviusis split to a seperate thread with the subject SIMATIC S7-200 - Communication with Sinamics G120. Best regards CS Moderator |
|
My Forum is the place to personalize your profile, |
|
Follow us on