Industry Online Support
Technical Forum
6/25/2010 11:08 AM | |
Joined: 1/4/2010 Last visit: 5/2/2024 Posts: 650 Rating: (40)
|
Hi you can Backup the archive in file: https://www.automation.siemens.com/mdm/default.aspx?DocVersionId=16484426123&TopicId=3463218315 And then you can start the burn program perhaps über a Button in WinCC: ProgramExecute("C:\\Program Files\\???\\??.exe"); The burn program will say if the the disk is full. Perhaps you can use DVD-RAM and write directly on DVD. |
Regards |
|
6/11/2011 5:20 PM | |
Posts: 947 Rating: (45) |
Hello davkav Use DLA (drive Letter Access)from Roxio. This programm allows the use of CD/DVD as hard disk. See also http://www.argentuma.com/backup/software/dla.html |
Last edited by: gre_m at: 6/11/2011 5:24 PM |
|
Follow us on