(0)| 6/30/2010 2:37 PM | |
|
Posts: 3 Rating:
|
I have ran into similar problem even I don't use the script at all. Here is my setup: Internal tag "Selector" that has 10 LinearScaling functions (for another 10 internal tags) on "Change Value" event. 10 buttons on the screen has SetValue function on "Press" event, each button set the value of internal tag to 1, 2, 3... up to 10. 11 field I/O indicators on the same screen showing "Selector" tag and another 10 tags used in LinearScaling functions. So, when I press the buttons I can see that the "Selector" tag value changes from 1 to 10 but LinearScaling tags not being updated. But... There is always BUT.... When I start the runtime with simulator and changing the "Selector" tag value from simulator the LinearScaling tags updating properly. So the question is: Is the event "Change Value" happens on external value chage only??? Splitted from Change Value event for internal tags . |
Last edited by: O_Moderator at: 6/30/2010 2:43 PMnew subject after splitting Last edited by: viktar at: 6/30/2010 2:43 PM |
|
Follow us on