(0)| 7/7/2010 1:19 PM | |
|
Posts: 661 Rating:
|
There is one problem: LOGO! has no stop watch function. Of course you can start and stop a timer (e.g. on-delay) depending on a threshold, but if it is stopped, the elapsed time is set to zero. So you could always see only the running time. I think what you need is a selfmade stop watch. Some time ago, there was a solution in the german forum (thanks to Betel Please see the attachment. You only have to modify the min/max parameters in the a. threshold triggers B016 and B018. And you have to think about when the time shall be reset (I3). Maybe when the pressure is <1.5 bar? To be able use the stop watch without analog value i kept I1 and I2. AttachmentStop watch in ms.zip (594 Downloads) |
| 7/7/2010 9:24 PM | |
|
Posts: 6 Rating:
|
Now i understand better why I didn't found the solution .. Thanks a lot for your help. This is exactly what I was looking for ! Have a nice day |
| 7/7/2010 9:26 PM | |
|
Posts: 6 Rating:
|
Do I have to do something to let know that I get the answer to my question and that the Topic is closed ? |
| 7/8/2010 8:51 AM | |
|
Posts: 661 Rating:
|
I agree. Unfortunately not everyone gives feedback like you did. |
This contribution was helpful to
|
|
Follow us on