(0)| 7/20/2010 2:38 PM | |
|
Posts: 211 Rating:
|
1. Scalance X101-1LD is a media converter (1 FO port single mode, 1 port wired RJ45 - see manual page). I intend to use it at line ends. OK? 2. HMI's will show only local station data. Three PC stations will show ALL data. 3. What about IP cameras? No problem if PC network card, with SOFTNET driver is used? And, thanks everybody. AttachmentScalance X100-200 pg53.pdf (341 Downloads) |
| 7/20/2010 3:13 PM | |
|
Posts: 5822 Rating:
|
Hello, regarding your first question I can tell you that the use of the media converter X101-1 LD at the end of the fiber optical line structure is absolutely normal. There is no problem with it. |
Follow us on