(0)| 7/23/2012 2:26 PM | |
|
Posts: 40 Rating:
|
Hello luliam, IhopeI will help you with my suggestions: first: go to properties -> network properties of your pc, and right click onthe connection you use betweenPC and LOGO! and choose properties: here you have to change theIP Adress of your connection so that the only differenceto the IP Adress of your LOGO! are the last digits, f.e.: LOGO! :192.168.1.10 Network connection: 192.168.1.11 Thenin the optionsof LOGO! Soft Comfort Software you have to set up also the IP Adresses: Look at this article: http://support.automation.siemens.com/WW/view/en/56348902, on step 1 until step 13. In Step 6 you see there is a button "detect".With this you can test if your connection between LOGO! and PC is succesful. If you have more questions, I would be glad to help you. Greetings, mika |
Follow us on