(0)| 8/8/2010 11:34 AM | |
|
Posts: 22 Rating:
|
Dear All, I've a problem with CPU 313C-2DP, i've just bought it for training purpose and i was testing it....i've made a simple program with ladder which is when every input (I0.0 ... I0.7 & I1.0 ... I1.7) makes an output (Q0.0 ... Q0.7 & Q1.0 ... Q1.7) to be energized...everything till now is going great...i went online and no commnuication problems occured...i began to apply my inputs one by one and monitoring the outputs...but the problem is that whenever i apply an input it's green led indicates that he's ON and no output comes ON, and when i tried to monitor these from STEP7 program....nothing appears also. I tried to force the outputs but invain.... Does anyone has an explaination to what happened with me? P.S. the program i used is in attachment thanks in advance. A.W AttachmentTest Prog.zip (202 Downloads) |
Last edited by: O_Moderator at: 8/9/2010 8:34 AMprogram attached |
|
| 4/26/2012 6:43 AM | |
|
Posts: 69 Rating:
|
Check Attchment For More Detials Uncheck the system default and change it I124.0 to I0.0. |
| 9/12/2016 11:07 AM | |
|
Posts: 23 Rating:
|
how the system default addressing starts with I/Q124 instead of I/Q 0
|
Follow us on