9/2/2010 2:01 PM | |
Posts: 137 Rating:
|
PLEASE i wait your replying HELP Maher
|
9/2/2010 11:09 PM | |
Posts: 137 Rating:
|
Hi please give the steps to do it thanks a lot for your supporting Best regards Maher
|
9/3/2010 7:50 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello Maher, Look at attachment. Best regards, Hristo Mihalev Attachmentsteps.zip (522 Downloads) |
9/5/2010 5:49 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, You can't to upload drive's parameters via CPU. Idea is when you are connected to the CPU (MPI, Profibus, Ethernet) means PC is connected, using the same hardware connection - to make possible to reach the drives (connected with profibus to the CPU). For this purpose you need Delivery release for Drive ES Basic V5.4 SP5 .(You could use lower version but it depends from types and version of your drives). Take a look at Routing with DriveES Basic (STARTER or DriveMonitor) in a STEP 7 multiproject. and Routing among PROFIBUS subnets on one CPU 400 using the DriveMonitor of DriveES and Routing for MASTERDRIVES. Then just use my steps from previous my post. Best regards, Hristo Mihalev |
8/22/2011 4:42 PM | |
Posts: 2 Rating:
|
Hi, I Connect 3 MOTORS [1FK7063-5AF71-1SA0], to 3 MasterDrive MC [AC/AC DRIVE 6SE7021-0EP50] & communicated wit CPU 315-2dp I set same PARAMETERS with Drive ES & Drive Monitor,Now after Start with same signal. Drive is Enable & Motor is Locked but i can not run the motors. And I don haveConstant FWD & BWD Parameter.[is changed without any thing] I send you same PIC for my setting. PLZ,Where is my Point andi want start MOTORS by Esay way,[It means with MasterDrive MC OP] Please send me STEP by STEP,COMMUNICATION,PARAMETERS SIGNALS & ...for start motors. Regards, Ashkan AttachmentMC setting.zip (505 Downloads) |
Follow us on