(0)| 9/23/2010 10:11 AM | |
|
Posts: 25 Rating:
|
Please , help me ! Thank you in advances! |
| 9/23/2010 5:33 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello Michele; You could do it in3 ways that I know of (and one is very very recent, so the information in not very well documented): 1) use a Siplus RIC bundle (Siemens PLC + MMC+special protocol drivers for IEC 60870-5-101/104) to interface between your WinCC and the external supervisor program: https://www.automation.siemens.com/mcms/topics/en/siplus/ric-telecontrol/bundle-s7-300/Pages/default.aspx 2) Member Pravin Patil has proposed a TIM 3V IE module supporting IEC 60870-5-104 comms in the following thread (look at the last post; the earlier ones discuss the modules presented above); he also suggests some links for more information: /tf/WW/en/Posts/48636#top 3) look at this recent press release describing WinCC Telecontrol software, that supports IEC 60870-5-104 directly from the WinCC PC: http://www.siemens.co.za/en/news_press/news2010/process_visualization_system_enhanced.htm I suggest you use the contact information at the bottom of the document to ask for more information. Hope this helps, Daniel Chartier Edit: I am afraid I know nothing about Triangle Microworks, besides what they state in their webpage. It seems they offer protocol development solutions, so you might be able to develop a IEC 60870 server on the WinCC PC that you could use to connect to the supervisor program, provided it is a IEC client. But you would have to exchange data with the WinCC program and the server in order for it to present information for the client, and that I could find no information on... Good luck on your project, D.C. |
Last edited by: dchartier at: 9/23/2010 5:41 PMLast edited by: dchartier at: 9/23/2010 5:35 PM |
|
Follow us on