Industry Online Support
Technical Forum
9/30/2010 9:02 PM | |
Posts: 15 Rating:
|
[schnippschnapp] second question is in the following thread what is the main benefit of using TSEND_C compared to TSEND?. how would be the best way in detecting if LAN cable is puled out of PLC so that connection can be restored after the cable is put back in PLC? I have to now make the PLC communication safe and reliable, means I have to monitor if there are some errors on the communication, if somebody cutted the cable, if.... So that I recognize this things and I act accordingly in my program. Thanks for the suggestions, Borut Splitted from Integrating two PLC communication in a programm. |
Last edited by: O_Moderator at: 10/4/2010 1:04 PMnew subject after splitting |
|
Follow us on