(0)| 10/6/2010 9:31 PM | |
|
Posts: 33 Rating:
|
Hi Guys I have two problems and possibiltities. [schnippschnapp] Second problem to do with the alarms.obviously, it is in groups. now, i set a bit in the plc of that particular word, it is looking at and something else comes on when the correct alarm does not. WHy is this? in other words i set bit m5.5 in plc for a low level alarm and i get a high level alarm which is on another bit. the inputs and wiring is 100% accurate, so i am lost? Help?!? Splitted from Alarms onHMI (KTP600) via s7 1200. |
Last edited by: O_Moderator at: 10/11/2010 9:45 AMnew subject after splitting Last edited by: Andy Moods at: 10/6/2010 9:34 PM |
|
Follow us on