(0)| 11/8/2010 4:48 AM | |
|
Joined: 10/7/2005 Last visit: 1/19/2026 Posts: 3054 Rating:
|
Hello R. Georgii unless you have downloaded the WinCC flex application with the "backtransfer" Option enabled I wouldn't worry too much about"protecting" the OP from an upload. Without the "backtransfer" Option enabled you (or your customer) will only be able to uploadthe compiled runtime file which is help- and useful to restore a panel in case it needs replacement, but can NOT be used to makeany changes to it (you can NOT open it with WinCC flexible) and you can find out more about this HERE. Any other restrictions to acccess the OP77B's OS and settings can be made from theWindows CE Control Panel (see chapter 6.2.3.5 of the OP77B manual). I hope this helps. |
|
Cheers |
|
Follow us on