(8)| 11/24/2010 2:38 PM | |
|
Posts: 19 Rating:
|
I have one question about WinCC, We are thinking about developping an application that will run in a PC to make the supervision of a production line and to other fonctionalities. We are looking which software is better to develop it. I've been reading about WinCC and it seems a really powerful tool. I'm trying to compare if It would be enough for us to develop our application with WinCC felixible and install it like a RT in the PC. Which are the main differences? Do WinCC applications allow to run more than one script at the same time? Does WinCC flexible running as RT allow it? Because for one past project we were working with WinCC flexible on a MP377 and one of the biggest problem was that we needed to wait that one script was finish to make another one start. Regards, Ignacio Splitted from WinCC supervisor cost. |
Last edited by: O_Moderator at: 11/25/2010 8:05 AMnew subject after splitting |
|
| 12/14/2010 10:10 AM | |
|
Posts: 37 Rating:
|
WINCC is a scada program like INTOUCH WINCC flexible was created to programm HMI, it s not a SCADA program |
Last edited by: seb_nancy at: 12/14/2010 10:11 AM |
|
| 1/29/2011 9:23 AM | |
|
Posts: 151 Rating:
|
hi friends you forgot a clear difference. wincc flexible commonly used for configuring hmi panels. but wincc don't support this part. clearly simatic wincc is better than wincc flexible for scada and pc based monitoring. good luck |
This contribution was helpful to
|
|
| 2/9/2011 12:50 PM | |
|
Joined: 6/29/2010 Last visit: 10/27/2022 Posts: 112 Rating:
|
Hi bermuda, You're right, but the comparation is between WinCC and Wincc flexible RT (running at PC). Only for reinforce, WinCC is a SCADA system and Wincc flexible is a softwarefor programming panels. |
This contribution was helpful to
|
|
| 2/10/2011 3:54 PM | |
|
Posts: 1275 Rating:
|
Hello, WinCC Flexible can be used for a smaller stand-alone SCADA system, with limited functionallities. It can monitor variables, you can have screens and scripts. However the data export and connectivity options are definitely not like WinCC. It also hasless options andcan handle few tags. If you need scripts, extensive reporting or connectivity go with WinCC! Best regards, Danielle |
This contribution was helpful to
|
|
| 8/24/2011 6:38 PM | |
|
Posts: 3 Rating:
|
Many thanks! |
Follow us on