1/13/2011 10:11 PM | |
Joined: 12/14/2010 Last visit: 6/28/2023 Posts: 160 Rating:
|
Greetings Bizur responding to your first question, I carried out an observation of the record of use of the CPU with the task manager when executing the WinCC with the DAP active and surprisingly the use is minimum (with very brief picks), there is not overload of the CPU; regarding the second question, I use the DAP to try to accelerate anyone of my discharges because I don't have a lot of band width. [schnippschnapp] new question is splitted to why I cannot consent to the configuration of the CCAgent for the way that siemens suggests ?. best regards |
Last edited by: O_Moderator at: 1/17/2011 8:32 AM |
|
1/31/2011 10:42 AM | |
Joined: 10/3/2010 Last visit: 7/31/2024 Posts: 1560 Rating:
|
I have exact the same error "AP Connect failed , Error: The script control was not started." since last friday. It happened after doing some changes with the Configuration Tool. At first, everything looked fine after starting my project. After stopping the project and opening Graphics Designer, I get this warning several times. Also on stopping RT, it hangs now on "Deactivating - CC_Project_Date" Script Server at 69%... The "AP Connect failed"-message toggles several times with another Error-window "The system cannot find the file specified"... Other projects on the same PC work fine. Duplicates of this project on another PC give the same error-windows, so I'm pretty sure Configuration Tool (or me) messed things up between the WinCC-project & SQL ? If someone knows more things to try, please let me know. Thanks in advance. |
Last edited by: SteBo at: 1/31/2011 10:45 AMB r g d s , |
|
Follow us on