(0)| 1/2/2011 8:54 AM | |
|
Posts: 594 Rating:
|
https://support.automation.siemens.com/WW/llisapi.dll?aktprim=0&lang=en&referer=%2fWW%2f&func=cslib.csinfo&nodeid1=16604318&siteid=cseus&treeLang=de&groupid=4000003&extranet=standard&viewreg=WW&nodeid0=32027210&objaction=csopen |
This contribution was helpful to
|
|
| 1/2/2011 9:27 AM | |
|
Joined: 10/17/2007 Last visit: 1/9/2026 Posts: 4571 Rating:
|
================ Yes, MBA is right, for detail check "SINUMERIK System 800, Universal Interface, Planning Guide" make it simple, you can set SD5010=00000100 for PLC on line;it is no use SD5012 for PLC on line, SD5010=00000000 FOR USING PCIN (input) SD5012=00000000 for PCIN (output) 810M/T can only use S5. HTH |
|
If you like my comments please |
|
This contribution was helpful to
|
|
| 1/11/2011 2:39 PM | |
|
Posts: 4 Rating:
|
Hi, i have continuos problem with serial communication with IOLAN to cnc. In the attached file i have inserti 4 image about the 4 cnc in particular about data bit configuration for have help about configure it for correctly trasfer program. I create an xls file with 4 configuration of cnc and with interface usage to recive program. I have read in the manual about this error: Number of Alarm 18 " error Format V24" cause: the velocity of transmission is not correct effect: the transmission is interrupt, last block is not memorized rimedy : control data setting 5011/5013/5019/5021 and control trasmission baudrate Number of Alarm 23 " Error parity v.24 " cause: last caracter trasmitt present an error of parity effect:the trasmission v.24 is interruped l'ast block is not memorized rimedy: control data setting 5011/5013/5019/5021 please give me an help for setting data of cnc because i have a problem ;( why i trasmitt with serial of pc and all funcionally correctly and when i use iolan no ?! there are error in the data setting ? Now i use program WINPER for send program in machine and the configuration is inside the attached zip of this email. Thansk for attention and disponibility. Sorry for my bad english Tiziano Tomasoni AttachmentCnc.zip (654 Downloads) |
Last edited by: O_Moderator at: 1/11/2011 2:46 PMcontact data deleted Last edited by: 2tsolution at: 1/11/2011 2:41 PMMY SERIAL CNC CONNECTOR HAVE ONLY 3 PIN, PIN 2, PIN 3, AND PIN 7. ( TXD, RXD, GND) Last edited by: 2tsolution at: 1/11/2011 2:41 PMMY SERIAL CNC CONNECTOR HAVE ONLY 3 PIN, PIN 2, PIN 3, AND PIN 7. ( TXD, RXD, GND) |
|
| 1/11/2011 3:24 PM | |
|
Posts: 2964 Rating:
|
Hello...
program what your sending it control does it have header of % normally it should be.... check it out... can you try using parity EVEN and check ??? attaching yout the pdf of RS232 cable configuration check it out.... Regards, Ekalavya AttachmentRS232 serial cable.pdf (858 Downloads) |
Follow us on