(0)| 2/1/2011 6:31 AM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
I had WinCC v7.0 SP1 in the PC, when the WinCC project runtime is activated there is an error. The "pdlrt.exe error 01.jpg", "pdlrt.exe error 02.jpg", "pdlrt.exe error 03.jpg" screenshots are attached for the error reference. The graphics runtime is not opening due to this error eventhough the runtime is activated. Due to this error i have updated WinCC to v7.0 SP2 UP2. (the new installed version is attahced) Even after updating WinCC, the same error exists. Kindly suggest to rectify this error and to have the WinCC Runtime without any error. Attachmentpdlrt_exe error.zip (717 Downloads) |
|
Like it? Rate it! |
|
| 2/1/2011 7:00 AM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
Hello, Please check the diagnose files in the folder \wincc\diagnose. And then use Evaluation of messages in the WinCC diagnostics files Best regards, Hristo Mihalev |
| 2/21/2011 8:27 AM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
wheather uninstalling WinCC and re-installation of the same will solve the problem? |
|
Like it? Rate it! |
|
Follow us on