(0)| 2/6/2011 6:33 AM | |
|
Joined: 7/28/2010 Last visit: 8/31/2024 Posts: 184 Rating:
|
Simotion, Any machine uses incremntal encoder needs a reference point to reference the machine either to zero or any other value. Mostly a sensor is used as a reference point, sometimes the Z pulse of the encoder is used as reference point. In your case, the axis which the encoder is mounted on is rotational and has to go up to 360 to show one complete rotation has happened and it gets reset by Z Pulse. In Periodic Counting, counter goes up till it reaches Upper limit and rolls over unless it gets reset or loaded to another value. Regards, Behnam www.sigmaprocess.ca |
Follow us on