(0)| 2/15/2011 10:27 AM | |
|
Posts: 7 Rating:
|
Dear Sir/Madam,I want to use following hardware and software for one of my substation automation projects.1. Redundant Operator Work stations based on SIMATIC Rack PCs with two Ethernet interfaces each.2. Main Redundant Controller based on SIMATIC S7-400H with two Ethernet interfaces each. 3. PCS-7 as the main control and monitoring software for OWS 4. SICAM PAS as the gateway for collecting the data from all the IEDs based on IEC 61850 and to transfer it to PCS-7 via S7-400H.I want to install PCS-7 and SICAM PAS on both the OWS in redundant configurations. One Ethernet port of each of the Redundant WS shall be used by SICAM PAS to collect data from IEDs via a redundant Ethernet network based on IEC 61805 while the other Ethernet port of each of the Redundant WS shall be used by PCS-7 to communicate with S7-400H on standard Industrial Ethernet. In a similar way, one Ethernet interface of each of the redundant S7-400 Controllers shall be used to communicate with SICAM PAS based on IEC 61850 while the other Ethernet interface of each of the Redundant S7-400 Controllers shall be used by to communicate with PCS-7S7-400H on standard Industrial Ethernet. Is the above configuration possible and workable? [schnippschnapp] second question is splitted to Can a single PC station accommodate both the softwares i.e. SICAM PAS . |
Last edited by: O_Moderator at: 2/16/2011 9:13 AM |
|
Follow us on