(0)| 2/14/2011 8:18 PM | |
|
Posts: 223 Rating:
|
[schnippschnapp] Second problem : how to compare the hardware of a project? I did a test with two project starting with the same hardware and I compared the SDB-folder. Result : no differences. Then in one project I added a digital input card and compiled the project. After comparison : no differences. How is this possible. How can I reliably compare the hardware of two projects? On the other hand I was confronted several times in the past with comparing online offline the hardware of a project and the comparison reported differences. But when comparing manually in detail all part numbers there was no differences (also not in connection etc.) This situation makes it really difficult to do service on machines. Please advice me, thanks. Splitted from Compare programs. |
Last edited by: O_Moderator at: 2/16/2011 8:33 AMnew subject after splitting |
|
Follow us on