3/1/2011 11:29 PM | |
Posts: 89 Rating:
|
Hello, My question is if i can use from Simatic_NET_CP Library CP400 FC 50 / FC 60 (AG_LSEND and AG_LRECV) with S7300 PLCs? |
3/2/2011 1:01 AM | |
Posts: 1064 Rating:
|
The fc50 and 60 are for the s7-400 in the s7-300 use fc5 and fc6 |
3/2/2011 2:08 AM | |
Joined: 10/7/2005 Last visit: 6/16/2024 Posts: 3008 Rating:
|
Hello autom I agree in principle with playerslightadvise, there is however a rather oddexception to this rule which only applies with TCP connections and older S7-300 CP's (e.g. 1EX10) in which case youshould use FC60 instead of FC6. Attached isthe print out of the Step 7 help with more on this matter adn other useful info(you'll get to this via the inbuilt help for FC5/6 or 50/60). I hope this helps AttachmentFC's for SEND-RECEIVE interface.pdf (443 Downloads) |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on