(0)| 3/7/2011 11:57 AM | |
|
Joined: 4/24/2006 Last visit: 1/20/2026 Posts: 9106 Rating:
|
Like UMENCHO mentioned, you need 6ES7195-7HD10-0XA0. This bus unit is already part of 6ES7153-2AR03-0XA0
The 6ES7195-7HD10-0XA0 is to connect two Interface modules (2x IM153-2) The 6ES7 195-7HB00-0XA0 is an active busmodule to accommodate two 40-mm wide I/O modules. (So you need 1 busmodule 7HB00 to use two 40-mm I/O modules)
See the following link: http://support.automation.siemens.com/WW/view/en/26291781 point 1. P.s.: you will also need a Backplane to insert 5 busmodules (6ES7 195-1GF30-0XA0) And perhaps a 6ES7 195-7HA00-0XA0 to accommodate a power supply and an IM153 module. Best regards, Wizard |
Last edited by: Wizard at: 3/7/2011 11:58 AM |
|
Follow us on