Industry Online Support
Technical Forum
3/31/2011 2:28 PM | |
Posts: 5 Rating: (0) |
[schnippschnapp] Another question regarding connections is with the cpu. If I were to have a multiple rack system with 1 cpu connected to the racks through interface modules and then I also wanted to use a communications processor to talk to remote IO modules, how would I connect the cpu to the communications processor.I see that the profibus connector would be going from the cpu to the interface modules so how does the cpu connect to the CP? Splitted from I am looking for information on connecting S7 300 series IO modules. |
Last edited by: O_Moderator at: 3/31/2011 2:42 PMnew subject after splitting |
|
Follow us on