Industry Online Support
Technical Forum
4/28/2011 1:15 PM | |
Joined: 6/1/2010 Last visit: 4/10/2024 Posts: 160 Rating: (1) |
Dear Sir, Please make my confusion clear on above discussion. 1. Generate a bit in wincc as a pulse generator with fixed freq. whatdoes it means is i hav to create aTag before generating it into plc. and how could i give plse generator fixed frequency for this Tag. or tell me step by step solution please,i realy do this bcoz my plc location is also long from HMI. Regards Splitted from Connection Fault Between PLC and Wincc. |
Last edited by: O_Moderator at: 4/29/2011 8:25 AMnew subject after splitting A9K |
|
4/28/2011 3:33 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Check the attachment for a solution.Another solution which I have seen in some projects is :transfer pulse from PLC to WINCC and write it back to PLC.These are some possible solutions. regards Attachmentwincc_pulse.zip (309 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on