(5)| 5/11/2011 9:28 PM | |
|
Posts: 126 Rating:
|
The other day Pegaia posted a sample project showing motor drive control using Profinet from an S7-1200. I decided to throw together one similar in function for Profibus. I put this small demonstration project together using TIA Portal 11 Professional using an S7-1214 to control a MicroMaster 440 drive. The motor drive is configured with 2 PZD words and 4 PKW words. It is a very basic implementation similar in function to the USS library. The GSD file is included as part of the project. Off 2 and Off 3 need to be set true prior to setting RUN to true. The Speed_SP will accept values between +200.0 and -200.0 with the values being percent of motor speed. There will be Profibus support with the Basic version of the TIA portal when it is released. AttachmentS7-1200_MM440_Profibus_DP.zip (3762 Downloads) |
Last edited by: bakerjw at: 5/11/2011 9:31 PM |
|
This contribution was helpful to
|
|
| 2/24/2014 9:17 PM | |
|
Posts: 1 Rating:
|
it seems if I write a 478 in the control word the drive will run, or if i write a 479 the drive will stop? |
| 6/11/2014 12:17 PM | |
|
Posts: 176 Rating:
|
Question split into new topicsample application of MM440 - clarification for spee_sp. With best regards, Narrator1
|
Follow us on