(0)| 6/13/2018 2:38 PM | |
|
Joined: 9/27/2006 Last visit: 1/1/2026 Posts: 12479 Rating:
|
Hello iion; It would appear that one or more of the As-i slaves is not properly configured, often this could be an addressing error. Any active error LEDs on any of the slaves? Have a look at the conditions that make the Config error LED light up, in the screenshot below. Sinec S1 Master modules CP 2433- Siemens AG This manual also shows you how to read the address LEDs to know which slaves are active on the bus, and how to use the AS-i master to replace the address of a failed slave on a new module. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/13/2018 2:39:33 PMLast edited by: dchartier at: 6/13/2018 10:32:12 PMLast edited by: dchartier at: 6/14/2018 1:30:20 AM |
|
Follow us on