5/20/2011 7:57 AM | |
Posts: 691 Rating:
|
You can take Text List for the same and assign an internal Tag/Script to change your screens |
5/20/2011 8:02 AM | |
Joined: 5/28/2009 Last visit: 9/11/2024 Posts: 127 Rating:
|
Hiefka |
Regards, |
|
This contribution was helpful to
1 thankful Users |
5/20/2011 8:08 AM | |
Posts: 799 Rating:
|
Thanks MavEric, |
5/20/2011 8:49 AM | |
Joined: 10/3/2010 Last visit: 7/31/2024 Posts: 1560 Rating:
|
you can find an example here: /tf/WW/en/Posts/44560 |
B r g d s , |
|
5/20/2011 2:46 PM | |
Joined: 10/3/2010 Last visit: 7/31/2024 Posts: 1560 Rating:
|
In the above script what should i give there in ScreenWindow ? This one works here: [code]Sub SelIndex_OnPropertyChanged(Byval Item, Byval value) If ScreenItems("Combobox2").SelIndex = "1" Then HMIRuntime.BaseScreenName = "Home" End If If ScreenItems("Combobox2").SelIndex = "2" Then 'objScrWindow.ScreenName = "Index" HMIRuntime.BaseScreenName = "Index" End If If ScreenItems("Combobox2").SelIndex = "3"Then 'objScrWindow.ScreenName = "vb examples" HMIRuntime.BaseScreenName = "vb examples" End If End Sub[/code] if you have following pictures in your project: "Home.pdl" "Index.pdl" "vb examples.pdl" but in this case, the sceen containing the combobox will be replaced with the one that you choose in the combobox, so you have to repeat the same combobox in all 3 screens Otherwise you can also work with picture windows instead. |
B r g d s , |
|
This contribution was helpful to
1 thankful Users |
Follow us on