(1)| 5/26/2011 12:08 AM | |
|
Joined: 9/19/2009 Last visit: 5/10/2025 Posts: 460 Rating:
|
Hello everyone! I have a litle problem with the file GSD for Sinamic, I have download from but when I try to install, I have a warning that tell me the file has an error,you can see screenshot. I try to install for Sinamic S120 CU320-2DP 6SL3040-1MA00-0AA0. I have installed the same file but diferent language but this don´t appear in my tree HW If anyone can give me a clou. Thank you advanced AttachmentGSD.zip (1494 Downloads) |
|
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to
|
|
| 5/26/2011 10:58 AM | |
|
Joined: 9/19/2009 Last visit: 5/10/2025 Posts: 460 Rating:
|
Thank you Mr KSN! You are right! Now I have installed the file GSD, but I can´t see it. I have updated the catalog, but in my tree don´t appear. Do you know why? Thanks |
|
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
| 5/26/2011 11:01 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Check the attachment. Best regards, Hristo Mihalev |
| 5/26/2011 11:45 AM | |
|
Joined: 9/19/2009 Last visit: 5/10/2025 Posts: 460 Rating:
|
Thanks Mr UMENCHO I have proved your indication, but still don´t appear, I have changed between all the profile. I have update HW from internet, I am working with V5.4 sp5, my profile version 03.2009 Thanks
Yes Mr KSN, in spanish there is two folders with Sinamics, you can see the attachment. I am looking for the next Hardware SINAMIC S120 CU320, but I can´t find it. |
|
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
| 5/26/2011 12:03 PM | |
|
Joined: 9/19/2009 Last visit: 5/10/2025 Posts: 460 Rating:
|
Thanks, but if you can send me again your screenshot because is the same that you have send in the previus post |
|
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
| 5/26/2011 12:06 PM | |
|
Joined: 8/25/2006 Last visit: 1/15/2026 Posts: 2221 Rating:
|
It's my mistake. Attachment reuploaded. |
Follow us on