(0)| 6/25/2011 4:07 PM | |
|
Joined: 9/27/2006 Last visit: 12/31/2025 Posts: 12479 Rating:
|
Hello Sree; You will need to setup a Modbus RTU master in the S7-400 rack, which means inserting a CP 441-2 (with a Modbus master loadable driver) in the CPu rack, or a CP341 (with the same loadable driver) in a ET 200M Profibus slave, or even a 1SI Modbus module in a ET 200S system. The Modbus master program will vary a bit depending on the selected hardware. What hardware have you thought of using, at this point in the project? CP 441-2: http://support.automation.siemens.com/WW/view/en/22302279 CP 341: http://support.automation.siemens.com/WW/view/en/24284824/133200 Loadable driver: http://support.automation.siemens.com/WW/view/en/4072784 ET 200S 1SI: http://support.automation.siemens.com/WW/view/en/26263724 Hope this helps, Daniel Chartier |
Follow us on