6/27/2011 9:47 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
https://www.automation.siemens.com/net-static/Quickstart2009/quickstart012003/html_76/iwlan/drahtlos_daten.htm And this FAQ would clarify the issue - http://support.automation.siemens.com/WW/view/en/23584230 2 - Scalance W788 - 2PRO 1- Scalance W788 - 2RR |
This contribution was helpful to1 thankful Users |
6/30/2011 9:58 PM | |
Joined: 12/11/2009 Last visit: 9/8/2022 Posts: 243 Rating: (4) |
it's running now . thanks for helps umencho and ins . umencho is flying. like all the time. очень спасибо |
7/1/2011 12:51 PM | |
Joined: 12/11/2009 Last visit: 9/8/2022 Posts: 243 Rating: (4) |
I put a picture in pdf where u can see antennas. I'm using devices in factory. Firstly two devices were in my office. Test ok. I moved one of them to 50 meters away another office sometimes it works sometimes it does not. If I put it nearer to 5 meters it works, if I put it in away 5 meters it does not work. Later I will use it in factory for controlling a press machine from a crane. Distance will be little than 50meters but it must be safe until 100meters. I'm using devices in Albania. Please tell me from which list u check whether if 802.11a is allowed in my country because I may use this devices in another countries.Meanwhile I did not change country it says Germany I'm not sure if you mean transmit power with EIRP but I did not change default settings about them. You can see screenshot in pdf And if you use 802.11h I would advice to change the setting od the Alternative Channel to something further away from yourPrimary Channel (for example 140). Now it's 104 ok I will change it to 140 and try again. Attachmentscalance_antenna_settings.pdf (170 Downloads) |
Last edited by: Osman_ at: 7/1/2011 12:53 PM |
|
7/1/2011 1:00 PM | |
Joined: 12/11/2009 Last visit: 9/8/2022 Posts: 243 Rating: (4) |
I also have 1 piece MD720 antenna.But I think I can't use it with scalance
Attachmentmd720antenna.pdf (171 Downloads) |
Follow us on