(1)| 7/20/2011 1:45 PM | |
|
Posts: 48 Rating:
|
hello, i need the configuration for communication cable between pc and the simatic s5 plc. thanks Splitted from S5 - S7 Communication. |
Last edited by: O_Moderator at: 7/21/2011 9:25 AMnew subject after splitting |
|
| 7/21/2011 2:39 PM | |
|
Posts: 1742 Rating:
|
Hello, You do not specify to what interface of the S5-PLC you want to connect the PC. Let us assume it is on the programming interface. With the exception of older programmig units like PG685, PG7xx, modern PCs do not have TTY interfaces (but only RS232). You needa convertercable making the conversion RS232/TTY. The pin assignment for the PC converter (MLFB 6ES5 734-1BD20) is displayed in the in the attached document figure of the following FAQ: http://support.automation.siemens.com/WW/view/en/28284967. |
| 7/21/2011 3:50 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
/tf/WW/en/Posts/47986 |
Follow us on