(0)| 11/24/2006 2:40 PM | |
|
Posts: 198 Rating:
|
Hi everyone.. I want to ask you about my new problem which is about bpm and alarm logging.. when i start a wincc project, on the alarm controls it writes "not active " and the menus of picture tree manager can not be shown. so I tried to put a c diagnose on the first picture to see what is happining you can see it on the added files. I checked that I have rigth of admin and all simatic groups ... I created a new project from 0 and it isnt working again. I put also diag folder to attachment files but nothing there as far as I see. But when I tried many things I could see 2 interesting errors but its not always giving those errors. after many pushings I could get those errors :) 1 of these is is a dcom error I found it on event viewer The application-specific permission settings do not grant Local Activation permission for the COM Server application with CLSID {BA126AD1-2166-11D1-B1D0-00805FC1270E} to the user NT AUTHORITY\NETWORK SERVICE SID (S-1-5-20). This security permission can be modified using the Component Services administrative tool. 2 . is after millions of wincc project tryouts I saw that there is a file called events.log in wincc\diagnose folder which has only this linegscrt.exe : 24.11.2006 15:00:13 : SIMATIC HMI WinCC (GlobalScript Runtime): Error :Error at GTI APEndAct There is no connection to the script control. Possibly no connection setup took place. ANY COMMENTS ? AttachmentDiagnose.zip (313 Downloads) |
Last edited by: Ates at: 11/24/2006 3:34 PM |
|
| 11/27/2006 12:57 PM | |
|
Posts: 3149 Rating:
|
Hi follow the FAQ for solving the onerrorexute entries: http://support.automation.siemens.com/WW/view/de/22198106 http://support.automation.siemens.com/WW/view/de/22196773 http://support.automation.siemens.com/WW/view/de/12124767 nemo |
Follow us on