9/11/2011 2:22 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Dear Aymen ALOUI It is possible to use a function written in STL in a block which is being developed in LAD. Best regards |
9/11/2011 8:16 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello There are LAD examples in the STEP's sample projects.To access use File->Open->sample projects.Also check attachment for STEP7 getting started manual. Best regards AttachmentNew Folder.zip (72 Downloads) |
9/12/2011 10:10 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Dear Aymen ALOUI
To develop your LAD logic we can help you here.You can start writing your codes and ask when you encounter a problem. For WINCCFLEXIBLE,you can refer to this conference: SIMATIC WinCC flexible About the attached file, I download it without any problem. Also check this thread for ideas about measuring Total running time! TOTAL TIME IN HH/MM/SS FORMAT (HOUR/MINUTE/SECOND)I hope this helps Best regards |
9/12/2011 10:36 PM | |
Joined: 9/11/2011 Last visit: 9/10/2024 Posts: 53 Rating: (0) |
Thank you so much the problem is that IDM has prevented the download now it's going. |
Follow us on