(0)| 9/10/2011 9:44 PM | |
|
Posts: 18 Rating:
|
hi Everybody, I am using Analog Input Module 6ES7 331-1KF02-0AB0 is this module is compatiable with PCS7 V7.1 SP2 ? if not how can i use this module , but when i pepare hardware configuration it wont given me any error or warning. But at the time of compiling of CFC chart it shown some warnings related with module driver. will u help me regarding this....please best Regards, Ashutosh Splitted from PCS7 Hardware Compatibility. |
Last edited by: O_Moderator at: 9/12/2011 10:07 AMnew subject after splitting |
|
| 9/12/2011 11:56 AM | |
|
Posts: 836 Rating:
|
Hi, when you can configure that hardware in PCS 7 environment it should be compatible. Can you please post the log file from module drivers (in log dialog... the tab "module driver"). By the way... this manual lists moduls that are released for PCS 7 (meanwhile there should be more modules availabe... but the the manual wasnt updated yet): http://support.automation.siemens.com/WW/view/de/7215812/0/en |
Follow us on