9/15/2011 6:06 AM | |
Posts: 6 Rating: (0) |
At one of our plants wewere using SIMATIC WinCC (V6.0 SP-3), to communicate with S5 155U PLC(CPU948) on SINEC H1 Bus. This Wincc system is communicating on Sinec HI with existing S5 system through CP 1613. There are 2 such Wincc servers that communicate with the PLC. On one of the serversthePC hard disk crashed so we reinstalled WinCC and everything is working fine and we are receving the real time data from PLC except for the recipes. but The 2 Wincc servers are completely identical in all respects. The recipe( work diamater, gear ratio and so on)is working in the 1st server. The recipes used to work fine prior to the reinstallation. We are not able to load the recipes using this 2nd wincc server. When we look for 'ua' folder in the wincc project there exists no such folder in either of the servers. also under the user archive tab of wincc explorer under archives nothing is listed in any of the serevers. Despite of that the recipe works for the 1st server and not for the 2nd. Attached are the screenshots for reference Please help. Attachmentpass schedule _pdl.pdf (100 Downloads) |
9/16/2011 11:21 AM | |
Posts: 1530 Rating: (59)
|
Hello Abhijeetmm, just one simple point to check. Did you activate User Archive in Computer Properties of WinCC Explorer (Folder Startup). Best regards Bizur |
Follow us on