(0)| 9/24/2011 9:31 PM | |
|
Posts: 4 Rating:
|
Dear UE I try to configure the Atlas copco compressor GSD in hardware configuration after installation of GSD it is not showing in additional field devices, when i try to reconfigure it is giving me warning that file already installed you want to replace it. Also how to create the GSD and which manual you are talking about ((manual (chpt. 6, page 54)!))) can you attached the manual here or send me the link from where i can download that manual Splitted from How to program ATLAS COPCO. |
Last edited by: O_Moderator at: 9/26/2011 11:50 AMnew subject after splitting |
|
| 7/1/2014 7:29 PM | |
|
Joined: 9/27/2006 Last visit: 1/13/2026 Posts: 12480 Rating:
|
Hello mussadiq; Luckily for us, more threads on this subject are available on the forum, reflecting the hard work and experience of forum members.. You can try to locate more by using the Search box at the right of this page, if you need more information. See uel123’s sample program for communication to a Combo-P module in this thread: combox-p communication with siemens S7400 PLC And the gsd file for the Combo-p is attached to this thread by PRG3:
Configuration of an Atlas Copco ComBox-P as DP slave Hope this helps, Daniel Chartier
|
Follow us on