(0)| 10/10/2011 4:52 PM | |
|
Posts: 376 Rating:
|
Hello, are you sure that you have a TS Adapter V5.2? The Siemens order number for the TS Adapter V5.2 is 6ES7 972-0CA34-0XA0. Please check this. You find this order number directly on the TS Adapter. You uses at the function “Set PG/PC interface” also the correct driver? Please check this. An attitude or a parameter is not correct? Please take into account. MPI/DP Network A maximum of 32 nodes can be interfaced to an MPI/DP network segment. The total cable length may not exceed 50 meters. Using so-called RS485 repeaters, several network segments can be combined to form a network comprising a maximum of 127 nodes.The data signaling rate in an MPI/DP network is max. 12 Mbit/s. Notes! The TS Adapter V5.2 supports transmission rates to max. 1.5 MBit/sec. Is your transmission rate in the PROFIBUS-Network higher? Please check this. Notice all information in the manual. Here the link for the manual TS Adapter V5.x http://support.automation.siemens.com/WW/view/en/14053309 You write you uses the software TeleService V6.1. Have you installed a Service Pack? If no, please has a look here. http://support.automation.siemens.com/WW/view/en/48733294 Best regards Azteke0110 |
| 4/16/2014 1:36 PM | |
|
Posts: 340 Rating:
|
new question is splittet to TS adapter v5.2, i can't communicat with s7 300 |
Follow us on