(0)| 10/19/2011 7:19 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Did you receive any error? Best regards, Hristo MIhalev |
| 10/22/2011 5:41 AM | |
|
Posts: 5 Rating:
|
Hi, The WinCC Flex is the Standard version. The Panel is TP177micro. With regards, Alfed. |
| 10/22/2011 6:08 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello , Try it How can you reset WinCC flexible to the original status of the last installation? Best regards, Hristo Mihalev |
| 10/23/2011 7:13 AM | |
|
Posts: 5 Rating:
|
Hi, Does that mean program created under SP1 will not be compatible with SP2 ? and no migration possible ? Anyone can confirm ? With regards, Alfred. |
| 4/24/2012 1:07 AM | |
|
Joined: 4/24/2012 Last visit: 10/18/2024 Posts: 5 Rating:
|
Hello, I've got the same message box ( "...project created with an incompatible or beta version..." ) when trying to open a project that was created under WINCC Flexible 2008 SP1 ( I have SP2 Update 13 now installed ). I've already tried what you suggested here about resetting the installation status, with no luck. Should I ask the guy who originally created the project with SP1 to save it under a previous version of WinCC ( as explained here ) and see if then I am able to import the project in the old format ? Is there really an incompatibility beetween SP1 and SP2 of WinnCC Flexible 2008 ? Or maybe someone can at least explain us how to migrate a project from WinCC Flexible 2008 SP1 to SP2... Thanks in advance for your time to answer me, regards. |
Follow us on