(5)| 11/4/2011 10:47 AM | |
|
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi Osman_, I have seen this Profibus Connector in the One of the Automation Exhibition, they displayed this product with application, EPIC® Data PROFIBUS Connectors 90° LED Screw TerminalsIf you see the following link 3rd image, on left hand side you will find the white rectangle in which it will show you the LED indication,
|
|
Ammy |
|
| 11/4/2011 2:33 PM | |
|
Posts: 243 Rating:
|
Yes vipa connectors seems beautiful. Thanks |
| 11/5/2011 9:47 AM | |
|
Joined: 10/7/2005 Last visit: 12/29/2025 Posts: 3052 Rating:
|
HelloNavnag the Profichip EasyConnPB Plugs (VIPA and Procentec sell these too, but they simply rebadge the Profichip Plugs as far as I know)need max 30mA fortheir LED supply whichcomes from the 5V supply that is mandatory on eachdevices with Profibus DB9 connector (note that this 5Vhas nothing to do with A and B signal lines, but is also the one that is used for the active termination). Each Plug will as such also draw the max 30mA from the device it is attached (i.e.they are not in parallel on the bus). As the 5V is generated from the devices general 24V supply, it is the ultimatesupply for the LED current (at a lower current though being a higher voltage supply). On the note of them failing: I'm aware of 2 failures with the Profichip Plugs out of a a several hundreds used (e.g.my observednon representitive failure rate is well below 0.5%), but never investigated furtheras to the cause of the failure (and had other non LED Plugs fail too in the past). I suggest you inform your supplier or ideally Profichip directly about you rather high failure rate, as I'm sure they would like to know about it and investigate the cause (and let us know what they find out). |
|
Cheers |
|
This contribution was helpful to
|
|
Follow us on