(0)| 11/25/2011 4:29 AM | |
|
Joined: 11/21/2007 Last visit: 12/8/2025 Posts: 2326 Rating:
|
Hello Nashwa Which PLC you are using ? There are two possibilities of transferring the S5 program to an EEPROM. 1. You can load the program in EEPROM using the EPROM programming port built into a SIEMENS PG. Or use a Siemens External EPROM programmer. 2. You can also download the program to S5 90U/95U/100U CPU using your cable and then copy it to the EEPROM. Pl see the manuals a) S5 90U 95U - See Section 4.4.1 http://support.automation.siemens.com/WW/view/en/1091648 b) S5 100U - see Section 4.4.1 http://support.automation.siemens.com/WW/view/en/1091978 Hope this helps Cheers Navnag |
|
There is no such thing as the last bug in a program |
|
This contribution was helpful to
|
|
| 1/27/2015 10:53 AM | |
|
Posts: 4758 Rating:
|
|
Follow us on