(0)| 12/16/2011 7:21 PM | |
|
Joined: 8/9/2011 Last visit: 4/24/2025 Posts: 19 Rating:
|
Hello, Thanks for the reply. I'm using ladder programming. The DB is global. There is an example of using LAD in the help file: The following example shows the indirect indexing of an ARRAY component as an example of LAD. ARRAY is a three-dimensional ARRAY. "Tag_1", "Tag_2" and "Tag_3" are PLC tags of the "Integer" data type. Depending on their values, one of the ARRAY components will be copied to the "MyTarget" tag.
|
| 12/17/2011 11:26 AM | |
|
Posts: 1410 Rating:
|
Yes, you are right I have found it in new manual (SP2), this is something realy new. |
| 1/30/2018 8:05 AM | |
|
Posts: 8946 Rating:
|
Like dP already said: use SCL. |
This contribution was helpful to
|
|
Follow us on