(0)| 1/7/2012 11:12 AM | |
|
Joined: 4/14/2010 Last visit: 6/26/2025 Posts: 525 Rating:
|
Greeting, Can i diagnose CPU 6ES7 414-3XM05-0AB0 V5.3 status with System Diagnostic V4.0 or is require V5.0...??? when i start the wincc runtime CPUDIAG the ocx window show a mwssage "CPU connection broken" Could you explain how can i configure the FB 432 to get the date for CPU 400 Diagnostic..??? please describe the parameter for FB 432 see attached.. Can i programe this in STL or CFC package require..??? Thanks, Regard Attachment14.zip (157 Downloads) |
Last edited by: Sarfraz Bhatti at: 1/7/2012 1:43 PMMS |
|
| 1/10/2012 9:08 AM | |
|
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello, I'm not understand. Do you use SIMODRIVE? There is also the using of a FB432. Please see in this case the FAQ in refer to this link: http://support.automation.siemens.com/WW/view/de/19364531 With best regards |
Follow us on