1/9/2012 6:47 AM | |
Posts: 16 Rating: (0) |
Hi, Our client needs IPv6 compliant system, Is SCALACE X414-3E is IPv6 compliant ? If not do we have any switch which is IPv6 compliant. Regards Brij |
1/9/2012 8:08 AM | |
Joined: 10/7/2005 Last visit: 7/29/2024 Posts: 3012 Rating: (1054)
|
Hello obrij as far as I know the only IPV6 capable SCALANCE switch is the new SCALANCE XR-500. If money is not the issue, it will be able to do whatever you want to it do (rumours have it that it can even make a good cup of coffee ). I would however suggest to ask your Client why he thinks he needsIPV6 capable switches in an industrial automation network (the 10.0.0.0/8 private address range alone contains 16777216 unique addresses, surely this is enoughtocover his Plant?, see also THIS link for more). I hope this helps |
Cheers |
|
1/9/2012 11:59 AM | |
Posts: 16 Rating: (0) |
Thanks for the reply |
Follow us on