1/12/2012 4:06 PM | |
Posts: 3037 Rating:
|
Hello, Do you have tested this with direct communication via ethernet? See the following FAQ: Displaying data of SENTRON PAC3200 / PAC4200 in WinCC flexible via über Ethernet Tweety |
1/12/2012 6:58 PM | |
Posts: 4 Rating:
|
no i dont test it .. is it necessary ? |
1/16/2012 1:26 PM | |
Posts: 4 Rating:
|
winCC flexible/ WinCC supports communication protocols of laptop built-in WIFI adapter or not?
|
1/17/2012 12:04 PM | |
Posts: 3037 Rating:
|
Hello, Yes you can communicate with WinCC flexible via Wifi. The setting for your network is described in the following FAQ. How do you configure a connection between WinCC flexible Runtime (PC or Panel) and a SIMATIC S7-300 / S7-400 via Industrial Ethernet? You configure the Wifi in the network settingsin your computer not in WinCC flexible. Tweety |
Follow us on