Industry Online Support
Technical Forum
1/30/2012 3:19 PM | |
Posts: 4 Rating:
|
Hello, I tried the same library as aminadra, after the initialization i am getting return_init_ok but after the cmd_send_start is true i am getting return_send_aborted with the returnstatus 7030 (no sms in the MD720-3 memory). please could anyone assist. Thank you. |
Last edited by: O_Moderator at: 1/31/2012 9:37 AMLast edited by: O_Moderator at: 1/31/2012 9:37 AMnew subject after splitting from /tf/WW/en/Posts/50458#top |
|
1/31/2012 11:33 AM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating:
|
hi simone... the return-status 7030 belongs to the receiving-routine. but you told us you are starting the sending-routine (cmd_send_start) and getting an error with return_send_aborted. So please write us what is the return-status of the sending-routine (must be a 8xxx-number). By the way: The 7030 is a valid termination of the receiving-routine. see http://support.automation.siemens.com/WW/view/de/40616248--> library description --> table 4-1 ".... x This is a valid termination of the RCV routine if there is no SMS in the memory of the modem x If you receive this status although there should be one or more SMS in the modem, check the memory of the modem manually with hyper- terminal and with the AT+CMGL command x If the SMS is really present in the memory of the modem, then save the “com_DB[DB154].compare_string” variable at the time after a RCV routine. Post this string in the forum of the Service&Support portal in combination with the used modem, hardware status and firmware status ..." verify that your sending-routine-status is not overwritten by the receiving-routine-status by setting "cmd_rcv_start_interval" to "0" and don´t trigger "cmd_rcv_start". cu |
Follow us on