(0)| 2/3/2012 9:45 AM | |
|
Posts: 186 Rating:
|
Dear all, I am trying to communicate two flexiblep roject in different system through OPC. i have made one as OPC server and another as OPC client. Problem is that i am not able to access OPC server tag in my OPC client project. may be some setting i have not configured due to which not able to access OPC server. for problem view, attaching a file Attachmentscrrenshots.zip (442 Downloads) |
| 2/3/2012 10:47 AM | |
|
Joined: 4/24/2006 Last visit: 12/24/2025 Posts: 9094 Rating:
|
Hello, Perhaps the following links might help: Which settings are required in Windows XP SP2 and WinCC flexible for server-client communication via OPC-DCOM? Which settings are required in Windows 2000, Windows XP, Windows Vista and WinCC flexible for server-client communication via OPC XML? Best regards, Wizard |
This contribution was helpful to
|
|
| 2/6/2012 12:11 PM | |
|
Posts: 3037 Rating:
|
Hello, Which WinCC flexible Version do you use? Which operating system do you use on your computer? Do you have test this with the sample project of this FAQ? Which settings are required in Windows XP SP2 and WinCC flexible for server-client communication via OPC-DCOM? Tweety |
Follow us on