(0)| 3/13/2012 9:57 AM | |
|
Posts: 3037 Rating:
|
Hello, You should use a "crossed" Ethernet cable(direct connection)for connection between your computer and your MP377. You can find more information abaut Reset to factorysettingsin the chapter 1.3 in the manual two in the following FAQ. How do you do an operating system update (OS update) on operator panels? What settings do you have to make on an MP 377 to reset the operator panel to the factory settings? Tweety |
| 3/15/2012 11:01 AM | |
|
Posts: 3037 Rating:
|
Hello, You should use MMC. Youshould not use MMC plus. You can findrecommended memorycard in the following FAQ. Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have? Tweety |
Follow us on