Industry Online Support
Technical Forum
3/26/2012 2:24 PM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating:
|
Hello Rajkiran, What you have Define in the CP341 Parameterization ? e.g. MODBUS Master, MODBUS Slave Have you able to get the Parameters... Button Enable on the CP Properties ? if not then Download the Following Software & installed to Enable it ... Download CD "CP340, CP341, CP440, CP441" & if you are going to Used Modbus master then Download Following Software Loadable Driver "Modbus Master (RTU)" if you are going to Used Modbus Slave then Download Following Software Loadable Driver "Modbus Slave (RTU)" |
Ammy |
|
Follow us on