(0)| 3/26/2012 1:35 PM | |
|
Posts: 10 Rating:
|
Hello everybody I have achieved a communication between "Logo! 0BA7" and "PC Access", as you can see at the attached files. Thank you in advance!!!
AttachmentSAMPLE PCACCESS-LOGO!0BA7.zip (1158 Downloads) |
Last edited by: Fotis at: 3/26/2012 1:56 PMLast edited by: Fotis at: 3/26/2012 1:36 PM |
|
| 3/27/2012 7:17 AM | |
|
Joined: 3/21/2006 Last visit: 10/16/2025 Posts: 10239 Rating:
|
Hello, I am assuming that is possible to use Simatic Net OPC (http://support.automation.siemens.com/WW/view/en/14587200) too. Just take a check which version of SIMATIC WinCC is released for which version of SIMATIC NET and which version of SIMATIC NET is supplied with SIMATIC WinCC is given in Entry ID: 21927773 . Instead of LOGO! assign S7-200 (like in How can you set up a connection between a LOGO! 0BA7 and an HMI Panel? ). And you need to have a extra license (SimaticNet) in order to supports more then 8 connections... Try it...But If the trick is much cheaper using PC Access... Best regards, Hristo Mihalev |
| 3/29/2012 3:06 PM | |
|
Posts: 2930 Rating:
|
Hi, there is no trick just add your 42 IP addresses to PC Access. The first chanel will be used automatically. Nothing necessary. regards |
| 11/15/2012 7:47 AM | |
|
Posts: 5 Rating:
|
Hello! Please, explain me! If in an example to change TSAP of the server, data exchange does not occur. All works only if TSAP 25.00. |
| 7/24/2015 10:58 AM | |
|
Posts: 4758 Rating:
|
|
| 8/12/2015 2:30 PM | |
|
Posts: 4758 Rating:
|
New question published by davidwill is split to a separate thread with the subject Siemans Logo 0BA8 to a Weintek MT8050ie HMI. Best regards |
Follow us on