(8)| 4/4/2012 6:41 PM | |
|
Joined: 9/24/2010 Last visit: 6/12/2025 Posts: 118 Rating:
|
Let me try more. Thank you so much
|
|
Mechatronic Center |
|
| 4/6/2012 8:58 AM | |
|
Joined: 8/31/2010 Last visit: 12/6/2025 Posts: 1525 Rating:
|
Hello Tranhieu0983, Enclosed is the Address in STEP 7 Classic and STEP 7 - TIA Portal v11. STEP 7 Classic: The red highlighted area in image "01_STEP 7 Classic" thas the addresses. STEP 7 - TIA Portal v11: The red highlighted area in image "02_STEP 7 - TIA Portal v11 - 02" has the addresses. In S7-1200 for having addresses in DB you have to choose Block Access as Standard, as shown in Image "02_STEP 7 - TIA Portal v11 - 01" AttachmentDB.ZIP (2535 Downloads) |
|
Like it? Rate it! |
|
This contribution was helpful to
|
|
| 3/16/2017 12:44 PM | |
|
Posts: 1 Rating:
|
Bit = "DBName".Tag.x0 Byte ="DBName".Tag.B0 This Tag is not working as I want to use bit of "int" type register |
| 3/16/2017 1:11 PM | |
|
Posts: 5521 Rating:
|
hi Swandra, this works only with the datatypes Byte, word and double-word. see the FAQ: Bewerten How in STEP 7 (TIA Portal) do you access the unstructured data types bit-by-bit, byte-by-byte or word-by-word and symbolically?hope this helps, regards, |
| 3/16/2017 1:29 PM | |
|
Posts: 243 Rating:
|
it works the same also for INT DINT SINT USINT UDINT data types.
|
This contribution was helpful to
|
|
Follow us on